Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

What to Look for When Specifying a Robot Cable
As industrial robotic applications become more and more demanding, we’re finding an increased need for flexible cables that can handle extremely complex movements and still deliver a long service life. When specifying cables for these types of applications, there are some important features to look for.

In order for a cable to withstand repeated torsional movement, it’s necessary for the cable to have a special design. It’s important that the conductors, shield construction and jacket materials of the cable compensate for major changes in bending load and diameter. To accomplish this, igus® uses "soft" structural elements—rayon fibers, PTFE elements or filling elements—that absorb torsional forces. When data transmission is essential, we use specially engineered insulation systems to ensure performance remains within a specified range over the cable’s service life.
Robot cables Figure 1: In contrast to conventional braided copper shields, a torsion-resistant, tin-plated copper shield sheath is used in igus®’ chainflex® CF Robot cables.
In contrast to conventional braided copper shields, a torsion-resistant, tin-plated copper shield sheath is used in igus®’ chainflex® CF Robot cables. The forces affected on the cable by any torsional movement are largely absorbed by sliding and buffer elements between the sheath, shield and insulation. Using a highly abrasion-resistant, halogen-free and flame-resistant PUR or TPE sheathing mixture prevents early failure of the shield and also protects the cable components from potential damage.
Robot cables in a multi-axis cable carrier on a robot Figure 2: Robot cables in a multi-axis cable carrier on a robot. igus®' CF Robot cables have been tested through more than 3 million torsional movements to +/- 270 degrees.

It’s also important to keep in mind that robot cables, unlike traditional continuous-flex types, can withstand various "mechanical stresses", including bending, torsion, centrifugal forces or a combination of all three. However, it’s nearly impossible to determine in advance what these cables can handle, even when taking into account their design or performance during use. So, to better evaluate these cables, igus® developed a "torsion test standard”. According to this standard, all CF Robot cables have been tested in the igus® test laboratory through more than three million torsional movements to +/- 270 degrees without failure.

Choosing cables for a robotic application can be challenging so paying close attention to a cable’s construction and working with a company that performs in-house testing can be key.

I’m interested in your thoughts about specifying cables in these types of applications. You can e-mail me directly at dnester@igus.com.

Useful Links


Application Assistance

For further questions or product information, please contact:

Photo
Sean Fournier

dryspin® Product Specialist

Email

Customer Service:

Monday to Friday from 8 am - 8 pm

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302