Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Plastic Bearings in Packaging Machine

A packaging machine that can produce up to 210 packages per minute uses iglide® plastic bushings from igus® to help guarantee quick timing and positional accuracy.

Design criteria: Lightweight and space-saving

A manufacturer providing various types of packages with a carrier handle uses a highly dynamic application head that has to be as lightweight and small as possible. The application head starts spontaneously on demand through a simple pressure-sensor system and provides up to 70 packages with a carrier handle in one minute.

The operation takes place in single-, dual- or three-track options - which means up to 210 packages are possible per minute.

To guarantee this quick timing and positional accuracy, the bearings used in the application head had to be lightweight and space saving.

iglide® plastic bushings and igubal® rod end bearings fulfilled not only these criteria, but helped to reduce manufacturing costs, lower the coefficient of friction, and enhance service life. They are lubrication- and maintenance-free, as well as vibration dampening.

The packaging machine uses iglide® G300 plastic bushings, which are economical all-rounders that can withstand high loads and chemicals. The self-lubricating effect means they are both maintenance-free and dry-running, as well as insensitive to dust and dirt. Coefficients of friction and wear rate are kept as low as possible.
Packaging machine bearings Packaging machine application head using igus® bearings and bushings
Said a spokesperson:

“For us, there was no alternative to igus®; taking into consideration the permissible weight, space and cost requirements. The decision to use igus® as our supplier made thing much easier for us. We had already worked with them many times before and the team there is always innovative and excellent at overseeing projects."

Useful Links



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302