Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Plastic bushings for electric scooter

Rear-wheel suspension

A new-design scooter uses an ultra-modern and effective electric drive tucked away in its carbon-fiber constructed interior. iglide® plastic bushings are used in the rear-wheel suspension and help enable a comfortable riding experience.

High loads

In fact, all the mountings on this innovative vehicle use iglide® plastic bushings, with the exception of the wheel bearings which use ball bearings.

iglide® Q plastic bushings are particularly well-suited to heavy-duty applications: they cope well with high loads and different pivoting angles.

Even in tough environmental conditions - like those encountered by an electric scooter out on the road - the igus® bushings are extremely wear resistant. This includes sub-zero temperatures, as well as heat and humidity. Even hard impacts as a result of potholes in the road, or the continuous vibrations do not affect the functionality of bushings.
Handle bar bushings iglide® Q high-performance plastic bushings from igus® are also mounted on the scooter's handle bar.
Scooter bushing iglide® Q plastic bushings are suitable for heavy-duty use and cope well with high loads.

More product information

More interesting applications from different industries

Useful Links



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302