Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Full-suspension mountain bike

Pivot points play an important part in rear-suspension design

A leading manufacturer of full-suspension mountain bikes has developed one of its most innovative bikes to date. Triple-butted tubing gives added strength to the joints, while the carbon-fiber frame is lightweight, corrosion resistant, and strong.

On the two front pivot points, between the swing arm and the frame, deep-groove ball bearings are used, because the bearings have to execute a relatively large swiveling motion. At the rear joint, on the rear axle, an iglide® J plastic bushing from igus® has been implemented.

The plastic bushing has a much larger contact area than a roller bearing. This means that, even under extreme stress and lateral forces, it doesn’t wobble.

To explore our bicycle industry page, click here.
Download the PDF version of this application story
bushings for bike The Bergamont ConTrail MGN

Selecting the optimal plastic bushing material

Originally, iglide® G300 plastic bushings had been considered. Bushings made from this material are suitable for the widest range of applications and are low cost. However, iglide® J provides greater dimensional stability when wet – a crucial parameter, if the bike goes through streams and puddles. The plastic bushing is inserted into the swing arm and enclosed in a metal sleeve, which forms the end stop for tightening the screws.
Plastic bushings on bike rear suspension At the rear hinge, on the rear axle, the bike's designers took a new approach by using a plastic bushing with a much larger contact area than roller bearings.
Mountain bike plastic bushing The plastic bushing is inserted into the swing arm and enclosed in a metal sleeve, which forms the end stop for tightening the screws.
Water resistant plastic bushings iglide® J provides greater dimensional stability when wet – a crucial parameter, if the bike goes through streams and puddles.

Specialist dealers and Olympic cyclists are fully satisfied

Dealers were extremely happy with the new solution because the feedback from bike owners turned out to be 100% positive. The torsional stiffness of the wheel is very good and the suspension responds very quickly.

Olympics winner Sabine Spitz won a gold medal in the Beijing Olympics in 2008 on a mountain-bike with iglide® plastic bushings in the suspension fork. The polymer components stood up to the constant impacts, edge loads, and dirt on the extreme course at the Chinese Laoshan Velodrome.

At the Athens Olympics in 2004 Olympics, mountain bikers who had ridden bikes with lightweight, wear-resistant iglide® bushings built into the guide rollers of the derailleurs, were awarded gold, silver, and bronze medals.

Browse Applicable Products

mountain bike plain bearing

iglide® G300 sleeve bearings

  • Most popular iglide® material
  • High wear resistance
  • Resistance to dust and dirt
  • Cost-effective
Shop now
mountain bike plain bearing

iglide® J sleeve bearings

  • Highly wear resistant on most shafts
  • Low coefficients of friction in dry operation
  • Vibration-damping
Shop now

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!

Contact an igus® expert now


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302