Cambiar idioma :
In addition to a drylin® linear system, numerous iglidur® bearings are also installed in this aircraft. No wonder, because the low weight of the plastic bearings is a decisive advantage over conventional metal bearings, especially in aviation. In this aircraft, the bearings are housed in the rudder and in the rotors, where they ensure that the aircraft can be easily navigated at all times.
Instytut Lotnictwa, Mirosław Delega, Warsaw, Poland

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas