e-chain and intelligent sensors for precision watering machinery with a span of 45m

Irrigation of potted plants on an area of 9,180m² saves up to 60% of water.

Profile

  • What was needed: a solution for condition monitoring of the energy chain
  • Requirements: The supply cables should run safely in a fail-safe guidance above the ground.
  • Industry: Agricultural engineering
  • Success for the customer: The safe and low-wear guidance in the e-chain enables a long service life, and the area below the cable guide can also be used for potted plants. As a result, the customer expects amortization of the investment after just four years.
The energy chain is a must in order to achieve the maximum use of space on the floor space of the precision watering [machine]. With the additional floor space gained, the investment in the energy chain pays off in four years. We are therefore happy to be able to use the energy chain here.

Peter Dercks

Dercks Gardening GmbH

Problem

Solution

Contacto

¿Preguntas o información sobre productos? Por favor, póngase en contacto con:

Profile
igus® México.+52 728 2843185Correo

Servicio al cliente