Cambiar idioma :
Thiessen Tillage Equipment has developed a cultivation system for vineyards, tree nurseries and orchards that enables rapid weeding between plants. The system not only reduces the use of herbicides, but also offers more protection for crops and a better harvest result, as it can adapt passively to changes in the soil contour. The system does not rely on electronics or hydraulics, but on the mechanical feedback of soil pressure. iglide® bearings are used in the system's parallel linkage, which allows the weed control head to float vertically depending on soil conditions. The device is now being used throughout North America and is beginning to make inroads in other countries around the world.

The device is mounted on the tractor and is therefore exposed to all weather conditions as well as sand and soil. There were three further problems for Thiessen Tillage to solve:
1. There is constant movement in the bearing points, albeit at low speed.
2. The bearing points are subjected to radial loads
3. The risk of failure due to insufficient lubrication
Initially, the company experimented with greased steel bushes and deep groove ball bearings. However, low-maintenance plain bearings were required that could be used easily and cost-effectively and withstand the harsh environmental conditions. So the decision was made in favor of iglide® plain bearings.
By using iglide® bearings, Thiessen Tillage Equipment was able to dispense with the use of grease nipples at the bearing points. The iglide® bearings also offered advantages in terms of design. By using them, the design and size of the mounting system could be adapted. For the end customer, they offer the advantage that they can be easily replaced in their own workshop if necessary.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas