Cambiar idioma :
An old water tower was converted into a central control room for monitoring the water supply. The room in the upper part of this tower is used as an education centre focusing on the environmentally friendly use of water resources and as a meeting room for the company management with its partners. As an aid for future educational purposes, six movable TV screens have been installed in two rows, which move around the room in a radius of 6.8 metres and at an angle of 180°. In addition, there are a further six movable TV screens in the upper meeting room, arranged in a single row. These TV screens move in a circle with a radius of 5.9 metres and an angle of 45°.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas