Cambiar idioma :
Industrial-grade USB cables for digital image processing
In digital camera technology, the USB interface has emerged as one of the leading standard interfaces. Responsible for transmitting large amounts of data without interference, it must stand up to mechanical stresses and the industry's high EMC requirements under all circumstances. For a clean signal transfer, one camera manufacturer recommends its customers use industrial-grade USB cables, which in the meantime can be used up to a length of 33 ft.
“It’s so easy!”, according to the company philosophy at IDS Imaging Development Systems GmbH, Obersulm. “Our compact cameras are aimed at the key customer benefit of easy installation and simple use in practice,” adds Marketing Manager, Thomas Schmidgall. “We pay attention to ultimate quality in this respect. That starts back in the development stage and ends with accessories!” For cameras that are used in tough, industrial image processing, IDS offers its customers USB cables from igus® as accessories, which are specially developed for the high demands on data transfer. For the dynamic movements in measuring and testing or for use in robots, the industrial-grade 'chainflex® CFBUS.065' and 'CFBUS.066' are recommended. “Their robustness and signal quality impressed us from the very start,” says the Marketing Manager looking back. “From a length of 5 m upwards, we only specify the industrial-grade cables from igus® for faultless data transmission. Conventional cables do not withstand the mechanical or electrical stresses over the long term. ” “For a very long time we looked for ways of implementing a transfer length of 10 m for industrial use, in order not to have to resort to any more interference-prone components. Before we came across the chainflex® cables, we tested a number of cables from a wide variety of suppliers. They did not stand up to any of the requirements of interference-free signal transmission. The USB connection itself was not the problem, but the mechanical and electrical stresses repeatedly caused failures.
The demands on the functioning transfer of the data are particularly high in visualization. “The signal quality is very good with the USB cables used. We did a variety of comparison tests beforehand; after a long search the igus® cables were the right solution; their quality impressed us,” says Thomas Schmidgall in closing.
Further interesting applications from extremely diverse areas can be found here.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas