80% less working time thanks to readychain

Pre-assembled energy chains save space and weight in this machine tool series.

Profile

  • What was needed: energy chain of type E4.1L, energy chain of type E4/light, both designed as pre-assembled readychain®, chainflex® cable
  • Requirements: As the machine takes up just seven square metres, the chains also had to fit into a small installation space. It also had to be assembled quickly.
  • Industry: Machine tool construction
  • Success for the customer: The pre-assembled chains save the customer 80% of the installation time. The first machine with the readychain® has been in operation 24 hours a day, six days a week for more than 18 months without any problems.
Machine tool UGrind 800 DD

Problem

Solution

At the heart of the UGrind 800 S (standard configuration) is the multifunctional head, which enables external, internal and face grinding, external, internal and face turning as well as measuring.

The igus® cable and energy chain are pre-assembled with connectors in the z-axis to ensure a reliable supply of energy and media to the multifunction head.

The x-axis also contains a ready-made energy chain from the E14 series. By using the readychains, DVS Universal Grinding GmbH was able to save 80 per cent of its working time.

Contacto

¿Preguntas o información sobre productos? Por favor, póngase en contacto con:

Profile
igus® México.+52 728 2843185Correo

Servicio al cliente