Cambiar idioma :
Whether bending simple or complex parts - with TruBend machines from TRUMPF, a wide variety of workpieces can be bent quickly and safely with maximum precision. For large and heavy parts, a bending aid supports the machining process. To ensure the safe energy supply of this support, TRUMPF relies on energy tubes from the R4.1L series from igus®.
"I personally have been working at TRUMPF for 25 years and cannot remember a time when we did not use igus® chains."
Volkmar Schmidt, Technical Purchasing Manager at TRUMPF Maschinen Austria
Decisive: A good mix of safe products and fast service
The mechanical load is rather negligible in the application of the bending aid, as the manual movement of the bending aid is not very dynamic. "However, the interior separation of the chain is all the more important for us in order to be able to lay all cables safely in their own chambers," emphasises Volkmar Schmidt. "This is where the expert advice on site comes into play, which really works very well with igus®. For smaller tasks, we sometimes design the chain ourselves online. For more complex things or prototypes, however, personal contact is important to us so that we can be sure that we are on the right track."
At TRUMPF, there are hardly any energy chains from igus® on bearing - as a rule, the company orders one to two days before production, whereupon the chains are delivered directly from the headquarters in Cologne in the appropriate length. Being able to rely on very good service here is very important for TRUMPF. "I personally have been working at TRUMPF for 25 years and I can't remember a time when we didn't use igus® chains," explains Volkmar Schmidt. A good basis, therefore, for the co-operation to continue for the next 25 years.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas