Cambiar idioma :
In the emergency room of a hospital, X-rays need to be taken quickly without having to move the patients. Here, the X-ray machine was mounted on the ceiling in a rail. This allows it to be used flexibly at any examination station. Previously, this application was not possible because cables hanging from the ceiling were in the way. Now the cables are guided in one of our roller e-chain® series 2828. As it has very low rolling friction, the X-ray unit can be moved quickly without any effort.
Xograph Healthcare ltd, Nigel Darwell-Stone, Tetbury, UK

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas