Cambiar idioma :
The company is an expert in the field of pioneering adhesive solutions such as anti-counterfeiting and anti-theft protection in the form of adhesive seals. The aim was to find cost-effective and maintenance-free ball bearings for use in conveyor rollers. There, the function of a deflection in the pressure roller before an intermediate drive was to be taken over. The pressure roller is set with a defined pressure force on the drive roller.
The combination of conveyor roller and intermediate drive not only serves to drive the product, but also generates web tension in the material, whereby different wrap angles can be set on the intermediate drive using the variable position of the conveyor roller. The different coatings of the rollers serve to protect the material as well as to improve material entrainment.
Alternative products

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas