Cambiar idioma :

Control cable for tightest bending radii ensures operational safety in low-floor trams
Public transport must be safe in all circumstances. There must be no interruptions in the running of operations. The focus is often on the doors. In this example, a cable used in a moving energy supply system ensures smooth opening and closing. Improved conductors and jacket materials make it possible that no more failures occur despite high continuous stresses.
The control cable is responsible first and foremost for opening and closing the doors in a controlled manner. This involves a part relevant to safety, which is sure to receive plenty of attention during all inspections. “To keep the costs as low as possible, we strive to only replace wearing parts with high quality, state of the art components,” explains Ernst Baerhausen. “And the longer the operating time of the cable, the more the maintenance intervals are reduced and thus our cost expenditure,” adds Hans Bennerscheid.
“The main difference to comparable cables lies in the conductor,” explains Rainer Rössel, Development and Marketing Manager for chainflex® and readychain® at igus®, in the interview. “Copper ages and becomes brittle over time. The CF98 cable is no longer purely copper, but instead a special alloy that is designed for a much higher mechanical stress. “
It features only a slightly lower conductivity compared to pure copper, which was compensated for by somewhat larger cross-sections – approximately 10 % bigger outer diameter compared to a comparable type. In view of the much higher demands of the last few years, it is certain, however, that such high quality solutions will be needed more frequently so that they can guarantee operational safety in the critical area of very small cross-sections. It enables new applications in energy supply systems – for example in the automation industry, the packaging industry, the mounting and semiconductor industry as well as the automotive and banking sector.
Cables for all applications
“Although we come from machinery and plant construction, our cables can show their strengths in many safety-relevant parts such as automatic doors in buses and trains,” Rainer Rössel points out. “Especially in the public transport sector, for example, we have been able to come up with solutions in some cases with very high tensile loads, which ultimately led to greater passenger safety, a higher availability and hence more cost efficiency. ” In the meantime, very many train doors have been fitted with our cables to ensure much higher reliability. As there is also no minimum order quantity or surcharge, follow-up costs are also reduced. Over 750 types of cable can be supplied from stock worldwide.
Further interesting applications from extremely diverse areas can be found here.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas