Cambiar idioma :
Profile
The xiros ball bearings are used in the planetary gears of a plastic planetary gearbox in a magnetic environment. The planetary gears work with the ball bearings at a close distance to the magnets. When the Savonius rotor rotates due to the effect of the wind, it forces the planet wheels to rotate both around themselves and around the central shaft. Increased rotations are transferred to the generator magnets via the sun wheel, as the crown wheel remains attached to the base. When the rapidly rotating magnets move close to the copper coils, electricity is generated.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas