Cambiar idioma :
The South Korean start-up MOBINN , which specialises in self-guiding robots, is focusing on the development of robots that can pick up deliveries and deliver them to a predefined destination. Load-mile delivery can be improved through the use of intelligent delivery management software that enables end-to-end transparency of delivery operations, automatic route planning and helps to centralise logistics data. Throughout the development process, our partners at igus® Korea have maintained close contact with their research and development department and provided several motion solutions. For the joint area of the wheel and the hinge mechanism of the robot body during its folding movement, we use iglidur® material. In addition, we use drylin® N in the transport guide inside the robot to minimise any irregularities during delivery. This minimises vibrations, shocks and friction on the outside of the robot while reducing the overall weight of the robot.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas