Cambiar idioma :
energy chain system in the grit chamber of the Bamberg sewage treatment plant
Increasing process reliability, minimising maintenance costs, future-proof data transfer - these are the requirements for the energy supply of the grit trap scraper at the sewage treatment plant in Bamberg. A reliable energy chain system from igus® ensures the necessary functional reliability. It replaces an ageing motorised cable drum. The cost-effective and low-maintenance complete system consists of a robust energy chain, various cables for power and data transmission and a stainless steel housing. Everyone involved is certain that the maintenance-free system will function trouble-free for many years to come.
"We are so satisfied that we are thinking of realising this chain on the primary clarifier scraper as well"
Rainer Mild, wastewater manager at the waste disposal and construction company of the city of Bamberg
The system has been running without any problems since it was installed in 2000. Maintenance costs have therefore been drastically reduced. It is therefore not surprising that the Aggerverband is satisfied with this solution. Those responsible also give the service from igus® good marks. Reinhard Braun, Head of Electrical Engineering at the Aggerverband, comments: "Our contacts have always responded quickly and unbureaucratically."
The lbt flizz® system has proven itself under adverse environmental conditions, and not only in this application. All the materials used in the system are corrosion-resistant and weatherproof. A correspondingly large number of other possibilities have already been realised, for example in rainwater overflow basins or harbour cranes, which have to meet extreme corrosion protection requirements. As the system components are also resistant to common chemicals, greases and solvents, igus® also supplies the lbt flizz® system to manufacturers and operators of galvanising plants and other chemical engineering facilities.

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas