Cambiar idioma :
Matthias Meyer presents the SCARA cable solution

White e-rib (standard black) on matching PMA corrugated hose
The reinforcement for existing corrugated tube systems. The e-rib is clipped onto the corrugated hose. The sizes are independent of the hose manufacturer. The e-rib stabilizes the corrugated hose so that it can only move in one direction. Thanks to the guide elements on the sides, the e-rib gives the corrugated hose an unsupported length.
For the SCARA robots, we offer nominal width starting at 29mm.
This video recorded at the igus® test laboratory shows how the SCARA cable solution works.
The ends of the SCARA mounted on ball bearings ensure an unrestricted rotary connection of the corrugated hose. The e-rib in conjunction with the corrugated hose provide stability so that the corrugated hose doesn't kink due to the movement.
In this video you can see the components if you opt for all three components of the SCARA cable solution.
The installation of the parts only takes a few minutes and is done with minimal use of tools.
You can find all the products shown in the video in the online shop:
The SCARA cable solution consists of three elements matching or adapted to the SCARA robot in question.
1: Moving end attachment (straight): TR.SCS.29.01.20.94.01.0
2: Moving end attachment (angled): TR.SCS.29.01.20.94.02.0
3: Fixed end attachment: TR.SCS.29.02.40.01.0
4: Corrugated hose with e-rib: TR.SCS.29.LLLL.0

The ESD SCARA Cable Solution consists of optimized, dissipative materials that enable use in ESD environments on the SCARA. The basic design of the standard SCARA Cable Solution, which forms the basis of the energy supply, has been tried and tested in the customer environment since 2020. Thanks to ESD certification, this system offers maximum safety in ESD environments.
The 3D printing material iglide® i8-ESD developed by igus®, which has high abrasion resistance and increased rigidity, serves as the base material for the connections. This specification guarantees secure and strong fastening of the connections.
The conductive corrugated tube in combination with the e-rib, which is also produced from ESD-capable material, completes the energy supply. The e-rib gives the corrugated tube sufficient stability, even in highly dynamic applications. In addition, a form-fit transition between the two end connections ensures certified discharge capability.


Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas