drone

Drone in a box

Lightweight, maintenance-free components for drone garages

The drone-in-a-box principle

  • A drone that can be automatically recharged - for example using charging contacts on the landing skids, a harness that you put on a normal drone, or an automated battery swap in the box.
  • The box serves as a take-off and landing platform for the drone. It is designed so that it can charge the drone or change the battery automatically. During the charging process or in phases when the drone is not supposed to be flying, the box serves as a safe storage location.
  • Control software plans and controls flight missions and routes.

motion plastics for the drone box

Drone box with igus products

Areas of application

  • In the security industry, the concept is used to automatically take off in the event of an alarm, fly to the location of the alarm and provide close-up images of the crime scene. Planned regular patrol flights are also conceivable. In addition, companies have already used the technology to support security at major events.
  • In agriculture, the concept is already being used successfully for inspection and surveying tasks. With special cameras on the drone, changes in vegetation can be recognised at an early stage.
  • In the maintenance of factories or power plants, drones in a box are used to stream aerial images and factory data to staff in real time. This can help to detect gas/water leaks, for example, or identify necessary maintenance.
  • Packing stations have already established themselves in many parts of the world as a practical option for time-independent parcel delivery. If these stations are expanded to include take-off and landing sites for drones, numerous parcel deliveries can be automated in the future.

Contacto

¿Preguntas o información sobre productos? Por favor, póngase en contacto con:

Profile
igus® México.+52 728 2843185Correo

Servicio al cliente