Cambiar idioma :
More on applied products here:
Customized special purpose machines for model- and mold-making
High-precision CNC machining centers
One of the focuses of the company is the development of CNC machining centers for model- and mold-making. These are mainly used in applications with high-precision work piece machining in both single and batch production. These machining centers master even the most demanding work on spatial bodies with absolute reliability. "It is an extremely universal machine concept by which both wood and plastic and also light metals and other typical modeling materials can be machined. ", clarifies Schell, the construction manager. Despite the elaborate design, standard parts are usually used in the customized machines. In the process, rugged plastic energy chains prove themselves to be reliable guides for the cables.
Suction hose instead of expensive housing
With a component or passage height of 500 mm, the customized machining center is altogether 3 m high. The travel distance in the X-axis amounts to 4.100 mm, in the Y-axis 2.600 mm, and in the Z-axis 1.000 mm. In the operation, speeds of up to 1 m/s with an acceleration of 5 m/s2 is implemented. Vacuum clamping devices that are universally used on the machine table provide the necessary flexibility while machining the parts. In this case it is used primarily for woodworking; the suction plays an extremely important role here. "The chips are not the problem in this environment, but the wood dust. It should not catch fire under any circumstances," explains the construction manager. A complete enclosure would be the safest, but also the most expensive solution. "For cost reasons, we have opted for a suction hose. " In order to do this safely and neatly, it has been housed in a special energy supply system as a customized solution. "This makes the machine even look pretty. “
Further interesting applications from extremely diverse areas can be found here:

Servicio al Cliente:
Teléfono: De lunes a viernes, de 8:00 a 20:00
Chat en vivo: 24 horas